Issue:
Product Features
Product Line:
CB Enclosure
Cause:
Clarification on product features
Resolution:
Yes, the NEMA Type 12, 12K, and 4/4X/5 stainless steel circuit breaker enclosures have an external operating handle located on the right side wall. The enclosed circuit breaker is operated via the external operating handle.
Released for: Schneider Electric Canada