How can we help you today?

Can auxiliary contacts be added to the 2510 Type M & T manual starters?

Issue:
Can auxiliary contacts be added to the 2510 Type M & T manual starters?

Product Line:
Manual Starters, Type M and T—Integral Horsepower

Environment:
Manual Starters and Switches

Resolution:
Yes, however for proper operation only 1 auxiliary may be added as outlined below:
Factory Installed - normally open Form X1 or normally closed Form X2.
Field Installed - normally open 9999SX11 or normally closed 9999SX12.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: