Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Form Y500 on the Class 8536SG* NEMA size 5 starter?
Issue:
Meaning of Y500 suffix on a 8536SG NEMA size 5 starter

Product Line:
NEMA and Definite Purpose Contractors and Starters

Environment:
8536 Type S starter

Resolution:
Y500 is an obsolete form which provided 300:5 current transformer and size 1 overload relay package on Series A devices. This Form is no longer required as the Series B devices are supplied as standard with this CT package.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings