Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement handle for a 9421FN1?
Issue:
9421FN1 replacement handles

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9421 Type L Circuit Breaker Mechanism

Cause:
Replacement parts

Resolution:
Current replacement operating mechanism will be a Class 9421 Type L operating mechanism depending on the old mounting depth:
Class 9421 LN1
Class 9421 LN3
Class 9421 LN4

NOTE: The customer will be forced to drill new holes in the door in order to mount the new handle because the shaft location relative to the old shaft position will be different.
A steel cover plate large enough to cover up the old handle mounting holes and provide a base for the new handle is strongly suggested. The new handle will not cover up all the old handle holes.

Detailed handle dimensional comparison between the old Type F and new Type L operating mechanism is available upon request by contacting the Customer Information Center at 1-888-SQUARED.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings