Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU661DS, series F6? (may be shown as F06)

Issue:
Repair parts list for HU661DS, series F6

Product Line:
Safety Switches

Resolution:
The repair parts for the HU661DS, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of "left side" and "right side" mean your left or right as you face the switch.)
-Line Base - one each of 4056792750 (left side base), 4056792650 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 for each line base)
-Arc Suppressor Assembly - 4056635550 (requires 1 for the left side, and 1 for the right side)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 - (2 required)
-Ground Lug Mounting Screw - 4020513503

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings