Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H364DS, series F6 (may be shown as F06)?

Issue:
What are the repair parts for the H364DS, series F6 (may be shown as F06)?

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H364DS, series F6 (F06) are as follows. No other parts are available:
-Complete Line Base - 4056703450 (requires one line base per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020514202 (requires 6 per line base)
-Load Base Assembly - 4056677450 (1 required per phase - includes phenolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020514202 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (Note: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (2 required)
-Handle Assembly - 4056736850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056738901(also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screws - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings