Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the dimensions for a XALK174 Control Station?
Issue:
XALK174 Control Station measurements

Product Line:
Harmony XALK 22mm Control Stations

Environment:
XAL 22mm Control Stations

Resolution:
The dimensions for the XALK control station are 2.68" W x 2.68" H x 2.09" D

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings