Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are replacement contacts available for the Class 8502 Type SE NEMA size three contactor?
Issue:
8502 Size 3 replacement contacts part number

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
Yes, Class 9998 Type SL6 for two pole or Type SL7 for three pole devices.
If device is four or five pole it will be necessary to obtain two kits.

Schneider Electric Canada

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings