Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the control wire lead lengths on QO-PL breakers?
Issue:
What are the control wire lead lengths on QO-PL breakers?

Product Line:
QO Minature Circuit Breakers

Environment:
North America Distribution Equipment

Cause:
Additional product information

Resolution:
The standard lead length of the control wires on QO-PL breaker is 18 inches.
Longer lengths are availably by adding a 4-digit suffix to the part number.   The suffixes and lengths are:
5392 = 48 inches
5393 = 60 inches
5394 = 72 inches

Instruction Bulletin for the QO-PL breaker is attached.



CTA-ID : 2015533

Schneider Electric Canada

Attachment(s)
QOPL Breaker Instruction Bulletin 48840-49604.pdf [33.98 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings