Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the mounting nut that connects the QOM1 or QOM2 main breaker to the bussing in the QO and Homeline convertible load centers?
Issue:
Repair parts

Product Line:
QO and HOM LC

Resolution:
The part number for the keps nut used to tighten the QOM1 or QOM2 main breaker to the load center is 2342702001. A quantity of 2 are required for each QOM1 or QOM2 breaker.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings