Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the GV2ME and GV2P manual motor starters be used on a DELTA system?
Issue:
GV2ME and GV2P on a Delta system

Product Line:
Tesys GV Manual Starter and Protectors

Environment:
North American Products

Resolution:
When used as Manual Motor Controllers, GV2ME & GV2P can be connected to Delta distribution systems up to 600V. (wye systems up to 600V being also compatible). When used as Combination Motor Controllers type E or type F, GV2P (up to size 22 => 25Amps) can be connected to Wye distribution systems up to 480/277V but not to higher voltages or Delta Systems.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings