Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H461DS, series F6? (may be shown as F06)

Issue:
Repair parts list for H461DS, series F6

Product Line:
Safety Switches

Resolution:
The repair parts for the H461DS, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of left side and right side mean your left or right as you face the switch.)
-Line Base - one each of 4056626150 (left side base), 4056623750 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Load Base - 4056609350 (1 required for left side, and 1 for right side)
-Line & Load Base mounting screw - 4020515101 (3 for each line base & 2 for each load base)
-Arc Suppressor Assembly - 4056635550 (1 required for left side, and 1 for right side)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101652 - (2 required)
-Ground Lug Mounting Screw - 4020513503
-Fuse Pullers - FPK0610 (1 required for each line base)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings