Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If I change a Size 2 solid state overload mounted on an 8536 NEMA Size 2 starter to a Size 1 solid state overload, will it mount directly to the contactor?
Issue:
Identify if the overload can be downsized on an existing starter

Product Line:
Class 8536 NEMA Starters

Environment:
Square D NEMA Contactors and Starters

Resolution:
The standard size 1 solid state overload relay (9065SS110, 9065SS120, or 9065SF120) will not fit directly to a size 2 starter/contactor. Use the 9065SR112 (Class 10), 9065SR122 (Class 20), or 9065ST122 (Class 10/20). 2016276.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings