Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider offer an IEC contactor with contacts rated for 600 Vdc?
Issue:
Identifying a contactor for use up to 600Vdc

Product Line:
Tesys contactors

Environment:
Products sold and used in the United States

Cause:
600Vdc rated contactor needed

Resolution:
No, the maximum IEC rating for D- and F-line contactors is 460 Vdc. Contactors used on DC loads are not UL Listed.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings