Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are circuit breakers still available for the type MHP panelboard? Circa 1951 to 1959
Issue:
Are replacement breakers available for an MHP4227 panelboard approximately 40 years old?

Product line:
Circuit breakers

Environment:
MHP panelboards and breakers

Resolution:
This interior was manufactured between 1951 & 1959 and used type MM, M1, and M2 breakers.  All breakers and components are obsolete and no longer available.  The entire panelboard must be replaced.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings