Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the Domino DA01 16 mm contact block?
Issue:
Identify a replacement for the Domino DA0116 mm contact block

Product Line:
Harmony Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
Use ZB4BZ102 for metal operators and ZB5BZ102 for plastic operators functional replacement not phyical replacement.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings