Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Square D provide a two speed Tesys starter?
Issue:
Is a two speed Tesys starter available?

Product Line:
Tesys Starters

Environment:
IEC Contactors and Starters

Cause:
Need a two speed starter and would like to use an IEC style

Resolution:
We do not offer an IEC type multi-speed starter. Although it is possible to obtain two contactors and a mechanical interlock, it is not recommended and is not a supported application for this product. The class 8810 electro-mechanical or 2512 manual NEMA product line should be considered.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings