Does the XCKJ10541 limit switch have a neutral position, or is it right or left motion only?
Issue:
Identify if the XCKJ10541 limit switch has a neutral position
Product Line:
Class XCK Limit Switches
Environment:
Square D Limit Switches
Resolution:
The ZCKE05 head can be programmed to be at rest in the center position, left, or right. Remove the head and change the programming with the black knob underneath. This is not a neutral position, where one set of contacts changes when the lever moves left, and the other set of contacts changes when the lever moves right of center. To obtain a neutral position switch, ZCKJ404 is the body and head combination that would support this.
Identify if the XCKJ10541 limit switch has a neutral position
Product Line:
Class XCK Limit Switches
Environment:
Square D Limit Switches
Resolution:
The ZCKE05 head can be programmed to be at rest in the center position, left, or right. Remove the head and change the programming with the black knob underneath. This is not a neutral position, where one set of contacts changes when the lever moves left, and the other set of contacts changes when the lever moves right of center. To obtain a neutral position switch, ZCKJ404 is the body and head combination that would support this.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.