Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the number for the stainless steel rod, float, and stops kit for the 9036 float switch?
Issue:
Float Kit for 9036 Float switches

Product Line:
Pressure, Vaccum and Float Switches

Environment:
9036 Float Switches

Resolution:
It is the 9049A6CS. It includes a 7`` center hole #316 stainless steel float, 5` stainless steel rod, and 4 stainless steel stops.

Or.

9049A6S. It includes a 7`` tapped at the top #316 stainless steel float, 5` stainless steel rod, and 4 stainless steel stops.

Also 9038 switches

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings