Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for a GC100 / GC200 ground fault relay?
Issue:
What can I use to replace a GC100 / GC200 ground fault relay?

Product Line:
GC100

Resolution:
The GC100 Ground Fault relay is obsolete. It was replaced with a GC200 relay, which is now also obsolete and Schneider has no replacement.

If the GC100/GC200 was installed on a bolted pressure switch (Bolt-loc), then Services can replace it with a BPGF100.

If the GC100/GC200 was installed with a circuit breaker, then replace the breaker with one including integral ground fault protection. Services can do a retrofit to replace the breaker and the relay.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings