Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement autotransformer part number for the Class 8940 reduced voltage controllers?
Issue:
What is the replacement autotransformer part number for the Class 8940 reduced voltage controllers?

Product Line:
Class 8940 Pump Panels

Environment:
Motor Starters

Cause:
Replacement Components

Resolution:
Select from below based on specific controller:

Controller Replacement Transformer

8940RD4DV03   52911-071-51
8940RE1GV03   52911-071-59
8940RE4FV03   52911-071-59
8940RF4JV03   52911-071-59
8940RG1LV03   52911-071-68
8940RG1MV03   52911-071-68

8940VD1DV03   52911-071-51
8940VE1FV03   52911-071-59
8940VE2GV03   52911-071-59
8940VF1JV03   52911-071-59
8940VG2LV03   52911-071-67
8940VG2MV03   52911-071-67

8940RD2FV06   52911-071-56
8940RE2GV06   52911-071-60
8940RE2JV06   52911-071-60
8940RF2LV06   52911-071-68
8940RF2MV06   52911-071-68
8940RG3PV06   52911-071-72
8940RG3QV06   52911-071-76

8940VD1FV06   52911-071-56
8940VE1GV06   52911-071-60
8940VE1JV06   52911-071-60
8940VF1LV06   52911-071-68
8940VF1MV06   52911-071-68
8940VG4PV06   52911-071-72
8940VG4QV06   52911-071-76
8940VH1SV06   52911-029-52
8940VH2TV06   52911-029-52
8940VJ1WV06  52911-029-54

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings