Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the power terminal lug data for the LC1D80 and LP1D80 contactor?
Issue:
What is the clamp terminal wire size of LC1D80 and LP1D80 contactor?

Product Line:
IEC Contactors and Starters

Environment:
IEC TeSys D Contactor Accessories

Resolution:
For contactors with screw clamp terminals:
stranded cable w/o cable end : One #10-2 AWG or Two #10-4 AWG per terminal.
stranded cable w/cable end: One #10-4 AWG or Two #12-2 AWG per terminal.
solid cable: One #10-3 AWG or Two #10-2 AWG per terminal.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings