What is the power terminal lug data for the LC1D115 and LC1D150 contactor?
Issue:
Power terminal lugs for the LC1D115 and LC1D150 contactors
Product Line:
Tesys D Contactors and starters
Environment:
IEC contactors and starters
Resolution:
For contactors with screw clamp terminals:
stranded cable w/o cable end : One #8-250 kcmil or Two of the following per terminal: #8-1 AWG + #8-250 kcmil (one of each size range).
solid cable: One #8-250kcmil or Two of the following per terminal: #8-0 AWG + #8-250 kcmil (one of each size range).
Power terminal lugs for the LC1D115 and LC1D150 contactors
Product Line:
Tesys D Contactors and starters
Environment:
IEC contactors and starters
Resolution:
For contactors with screw clamp terminals:
stranded cable w/o cable end : One #8-250 kcmil or Two of the following per terminal: #8-1 AWG + #8-250 kcmil (one of each size range).
solid cable: One #8-250kcmil or Two of the following per terminal: #8-0 AWG + #8-250 kcmil (one of each size range).
Released for: Schneider Electric Canada