Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When an 8536 single phase starter is ordered, does it come with a 3-phase overload relay and a jumper strap kit from the factory?
Issue:
How will an 8536 Single Phase Starter looks like

Product Line:
NEMA and Definite Purpose Contactor and Starer

Environment:
8536 Magnetic Starter

Resolution:
It will have the center pole hardware on the contactor and overload removed and a single jumper strap is installed in the third leg of the overload relay. The customer will need to install one thermal unit sized per motor full load amperage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings