Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement lock for HCM Nema 1 panel trims?
Issue:
What is the replacement lock for HCM Nema 1 panel trims?

Product Line:
I-Line circuit breaker panelboards and accessories

Environment:
Replacement

Cause:
Selection

Resolution:
For Series 1 and 2 up to 38``: PK4FL

For Series E1 up to 48``: PK4FL if manufactured before 11/14/97. PK22FL if manufactured after 11/14/97.

For Series 1 and 2, 47`` and larger: PK5FL

For Series E1, 64`` and larger: PK5FL if manufactured before 4/5/02. PK22FL if manufactured after 4/5/02.

ALL PANELS THAT MEET 1984 NEC WIRE BENDING SPACE REQUIREMENTS ARE SERIES E1.

Revised 3/29/04



CTA-ID : 2004309

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings