Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the GV2RT**?
Product Line:

Tesys GV Manual Starter and Protectors

Resolution:
Toggle operated thermal magnetic motor protector for use on motors with high peak currents at start-up or for switching the primaries of 3-phase transformers. Listed below are the thermal and magnetic setting ranges:

Values listed below are in Amps.
Controller Thermal Range Magnetic Trip (+/-20%)
GV2RT03 0.25 - 0.40 8
GV2RT04 0.40 - 0.83 13
GV2RT05 0.63 - 1.00 22
GV2RT06 1.00 - 1.60 33
GV2RT07 1.60 - 2.50 51
GV2RT08 2.50 - 4.00 78
GV2RT10 4.00 - 6.30 138
GV2RT14 6.00 - 10.0 200
GV2RT16 9.00 - 14.0 280
GV2RT20 13.0 - 18.0 400
GV2RT21 17.0 - 23.0 400


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings