Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the consumption of the control coil for 8502SD contactor?
Issue:
Looking for the Coil consumption of the control coil for 8502SD contactor

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S contactors

Resolution:
For 2 & 3 pole devices 311 VA inrush and 37 VA sealed for 60 hertz or 296 VA inrush and 36 VA sealed for 50 hertz. For 4 & 5 pole devices 438 VA inrush and 38 VA sealed for 60 hertz or 429 VA inrush and 37 VA sealed for 50 hertz.

This also applies to all 8536SD, 8538SD, 8539SD, 8606SD, 8630SD, 8640SD, 8702SD, 8736SD, 8738SD, 8739SD, 8810SD, 8903SP, 8940 Size 2 except ``NP``, 8941ND, 8941CD, 8941UD, and 8941DD devices.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings