Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the old KDL main circuit breaker and the current QDL main circuit breaker used in the QO 3-phase load centers?
Issue:
Product Design Features

Product Line:
QO Load Centers

Resolution:
The KDL main circuit breaker is obsolete and no longer used in the Square D, QO, 3-phase load centers. The current design, QO, 3-phase load centers uses the QDL main circuit breakers. The QDL breaker is NOT a replacement for the KDL breaker and cannot be used in the load centers that used KDL breakers.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings