Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU663AWK, series F6? (may be shown as F06)
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU663AWK, series F6 (F06) are as follows. No other parts are available.
-Line Base - 4056802150 (left side base), 4056802050 (right side base), and 4056702801 (plastic connecting cam) (arc suppressor not included)
-Line Base mounting screw - 4020515101 (6 total required, 3 for each line base)
-Arc Suppressor Assembly - HAS0610F (2 required; includes arc suppressor, mounting screw, and instructions)
-Lug Assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (also requires switch mechanism gasket 4056603201)
-Handle - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screw - 2299940562 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings