Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is form G26 on an 8536 starter ?
Issue:
Checking on form G26 on an 8536 starter.

Product Line:
NEMA Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
Factory modification of the enclosure for NEMA Type 3R applications. The modification consists of the addition of 1/8`` diameter drain hole(s) to the bottom of the enclosure. If the enclosure is not dual rated NEMA 12/3R, this modification will not be UL Listed.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings