Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the 8536SCO8 starter?
Issue:
Identify 8536 part number

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Magnetic Starters

Resolution:
Standard 5-pole AC Magnetic starter with standard 3-pole melting alloy overload relay. All poles are N.O.
It consists of a standard 3-pole starter with a 2 pole power pole mounted to the left side of the starter.
Typical application for this starter would be a Class 8810 consequent pole starter where one of the contactors must be 5 pole.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings