Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there terminal blocks for use with LR9D solid state overload relays?
Issue:
LR9D terminal block

Product Line:
Contactors and Overload Relays

Environment:
TeSys™ D Contactors and Overload Relays

Resolution:
LA9F103 can be used for this purpose; however, please note that the shroud is for use on the load terminals of the overload relay and is intended for use when the overload is directly mounted below the D-Line contactor. There is no shroud for the line side of the overload.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings