Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the Vario loadbreak switches rated for DC applications?
Issue:
Are the Vario Disconnect Switches DC rated?

Product Line:
Vario Disconnect Switches - GIC Product

Environment:
US Product

Cause:
Product Selection Options

Resolution:
The Vario switches do have DC current ratings for DC1 & DC2 through DC5 applications. Refer to page 6 of the attached document for additional information.

Please note that as these devices are suitable for DC applications but have not been submitted to UL for testing and therefore are not UL Listed or Recognized for DC applications.

Schneider Electric Canada

Attachment(s)
9421CT0301.pdf [10.7 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings