Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the mounting screws for Q frame breakers?
Inquiry:
What is the catalog number of mounting screws for QB Powerpact breakers (also applies to QD, QG, QJ, Q2)

Product Line:
Powerpact QB type breaker

Resolution:
The replacement screws are:
4812112150A for a 2P breaker, which comes with (1) 2" and (1) 3" screw.
4812112050A for a 3P breaker, which comes with (2) 2" and (2) 3" screws.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings