Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a 9001KS11B, 2 position selector switch a maintained contact type?
Issue:
Characteristics of 9001KS11B

Product Line:
Harmony 30 mm 9001 K Metal Push Buttons

Environment:
30mm Push Buttons

Resolution:
Yes, it is maintained contact.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings