Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is an RHN411B good for 24 VAC or DC control circuit?
Issue:
RHN411B control circuit voltage

Product Line:
Relays and Timers

Environment:
Level Detector Relays

Resolution:
The RHN411B has a 24 vac 50Hz control circuit. The 24 VDC version is an RHN412B

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings