Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does class 2601 reversing drum switches have an off position?
Issue:​
Off-position of a 2601 reversing drum switch

Product Line:
Manual Starters and Switches

Environment:
Class 2601 NEMA style Reversing Drum Switches

Resolution:
Yes, these switches are provided as standard with a maintained (field convertible to momentary only) operator. There are three positions; Forward - Off - Reverse.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings