Issue:
2510 FL1 Material options
Product Line:
Manual starters and Swiches
Environment:
2510 type F manual starter and type K manual switches
Cause:
Need a padlock provision handle guard for the 2510 type F or K in stainless steel
Resolution:
No, the 2510FL1 is only available in zinc plated steel with a clear chromate film finish.
2510 FL1 Material options
Product Line:
Manual starters and Swiches
Environment:
2510 type F manual starter and type K manual switches
Cause:
Need a padlock provision handle guard for the 2510 type F or K in stainless steel
Resolution:
No, the 2510FL1 is only available in zinc plated steel with a clear chromate film finish.
Released for: Schneider Electric Canada