Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Nema rating on a 30 mm potentiometer?
Issue:
30 mm potentiometer protection rating

Product Line:
Push Buttons and Operator Interface

Environment:
9001 Type K and SK Push Buttons

Resolution:
It has a Nema 4, 13 rating.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings