Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CU12L400CB, Series M02?
Issue:
Current Design Repair Parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056250650 (also requires insulator and rivets)
Meter Cover Insulator - 4056138202 and (2) 2430313190 (rivets)
Meter Cover Mounting Screw - 4020513001K
Load Center Cover - 4056258950
Load Center Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - 4056232801 (handles not included)
Utility Pullbox Cover Handles - (2) 2940101103 and (8) 2430315290 (rivets)
Utility Pullbox Cover Mounting Screws - (2) 4020513001K and (3) X1299 (sealing screws)
Load Center Interior - 4056250750
Load Center Interior Mounting Screws - (2) 2142217101
Interior Deadfront Trim - 4056233001
Interior Deadfront Trim Mounting Screws - 4020513001K
Meter Base Assembly - 21324CD
Mounting Channel - 4056142003
Factory Installed Main Breaker - QDL22200
QDL Main Breaker Mounting Pan - 4056235201 and (4) 2142720140 pan mounting screws
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings