Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a green neutral bonding screw for a QO or Homeline load center available, even if the load center catalog number is not known?
Issue:
Replacement green bonding screw part number corresponding to specifications.

Product Line:
Load Centers

Environment:
QO and Homeline load centers

Resolution:
For the more current Series S_ load centers, below are the standard bonding screws. BUT it is always BEST to first obtain the catalog and series number of the load center, because a bonding screw can be changed without notice.
  1. 4028344850K bonding screw and card for QO 8 through 42 circuit 150, 200, and 225 ampere main breaker and main lugs.
  2. 4028345850K bonding screw and card for:
    a. QO 12 through 24 circuit 100 ampere main breaker and 125 ampere main lugs.
    b. HOM 16 through 120 circuit 100, 125, 150, 200, and 225 ampere main breaker and main lugs.

    FOR OLDER LOAD CENTERS THE CATALOG AND SERIES NUMBER WILL BE NEEDED.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings