Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the cover screws and the screw posts for a NEMA Size 3 Type SE contactor or starter ?
Issue:
NEMA Size 3 Starter cover screws and screw posts replacement

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
Part number for the cover screw is 21916-16281 and the part number for the screw post is 31074-048-50.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings