Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement disconnect blade assembly for an 8538SEA23 series D?
Issue:
Disconnect blade assembly for an 8538SEA23 series D

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8538 Type S Combination Starter

Resolution:
The replacement switch base assembly which contains the blades is a 40567-774-50 (Obsolete).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings