Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What prevents an XB5 selector switch operator from rotating under heavy use?
Issue:
Needs to know What prevents an XB5 selector switch operator from rotating under heavy use.

Product Line:
Push Buttons and Operator Interface

Environment:
22 mm Push Buttons

Resolution:
An anti rotation plate ZB5AZ902 is offered as an accessory, which consists of a metal plate mounted between the inside panel cover and the plastic ring nut. The plate bites into the cover surface and is held in place by the nut. The contact blocks and light modules have a key that fits into the nut to prevent loosening.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings