Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H361DSWC, series F7 (may be shown as F07)?

!!!Confidential ContentIssue:
Repair Parts

Product Line:
HD SS

Resolution:
The repair parts for the H361DSWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056603950 (1 required; arc suppressor not included)
-Load Base Assembly - 4056604150 (1 required)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4053922550
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate Mounting Screw - 2194918121 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541000045
-Receptacle Mounting Screws - 4510280101
-Ground Lug - 4025101652 (3 required)
-Ground Lug Mounting Screw - 4020513503 (2 required)
-Fuse Pullers - FPK03 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings