Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On the NENL34060RD12 MG breaker, what is RD12?
Issue:
What is RD12 in  NENL34060RD12 MG breaker

Product Line:
Circuit Breakers

Environment:
Compact NSE Circuit Breakers

Resolution:
The RD12 suffix indicates the breaker includes a factory-installed black-handled direct mount rotary operating handle. The rotary handle can also be purchased as a kit to field install, part number 28050.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings