Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are alternate lugs available for the EZM3800FS Series M01?
Issue:
Product Design Features

Product Line:
EZ Meter-Pak Metering Equipment - EZM

Environment:
Alternate Main lugs

Cause:
Non-standard or larger wire sizes

Resolution:
Yes, the standard mechanical lugs will accommodate (3) 500 Kcmil AL/Cu wires maximum per phase and neutral.
For alternate lugs see below:
1) For (2) 600 Kcmil Al/Cu Maximum per phase and neutral use the AL800MA7 lug kit for the molded case switch and the MMLK250 lug kit for the neutral.

2) For (2) 750 Kcmil Al/Cu Maximum per phase and neutral use the AL800MA7 lug kit for the molded case switch and the MMSK2 Lug landing kit with (2) ILSCO Lugs, TA8002N(Purchased separately) for the neutral.
NOTE: For the MMSK2 Kit, this kit includes three lug landing pads, use only the two lug landing pads having the smallest offsets. Do not use the connector with the large offset. Attach the ILSCO lugs to the Lug landing pads and then to the neutral.

3) For (4) 350 Kcmil Al/Cu Maximum per phase and neutral use (3) AL1000MA for the molded case switch and the standard neutral Lugs that come on the device.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings