Issue:
Need to know what maximum current the internal overload relay contact can handle.
Product Line:
Contactors and Starters
Environment:
NEMA Type S Starters
Resolution:
The contacts are rated NEMA B600 which is as follows:
5.00 Amp Maximum Continuous Carrying Current.
Maximum Make Volt-Amp 3600, Maximum Break Volt-Amp 360.
Need to know what maximum current the internal overload relay contact can handle.
Product Line:
Contactors and Starters
Environment:
NEMA Type S Starters
Resolution:
The contacts are rated NEMA B600 which is as follows:
5.00 Amp Maximum Continuous Carrying Current.
Maximum Make Volt-Amp 3600, Maximum Break Volt-Amp 360.
| Voltage | Make (amps) | Break (amps) |
| 120 | 30 A | 3 A |
| 240 | 15 A | 1.5 A |
| 480 | 7.5 A | 0.75 A |
| 600 | 6 A | 0.6 A |
Released for: Schneider Electric Canada