Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I shorten the depth of a standard 9001KM light module and contact block mounted in tandem ?
Issue:
How to ensure light module will fit in a shallow depth enclosure?

Product Line:
30mm Push Button

Environment:
9001 Type K, SK, and KX Electrical Components

Cause:
The depth of a standard 9001KM light module is in question for a particular application.

Resolution:
Yes , use a 9001KM55 shallow depth light module which will mount side-by-side.  Standard 9001KM + 9001KA = 2.78 inches/ 70.61mm, Shallow depth 9001KM55 or 9001KM58 + 9001KA = 1.75 inches / 44,45mm.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings