What size is the mounting hole for the 9003K2 cam switches?
Issue:
Need to know the mounting diameter for the 9003K2 Cam switches.
Product Line:
Push Buttons and Operator Interface
Environment:
Cam Switches
Resolution:
All the 9003K2 front mounted cam switches can be mounted in a 22.5 mm hole. There are also some four hole mounting operators that can be used for rear mounting switches.
Need to know the mounting diameter for the 9003K2 Cam switches.
Product Line:
Push Buttons and Operator Interface
Environment:
Cam Switches
Resolution:
All the 9003K2 front mounted cam switches can be mounted in a 22.5 mm hole. There are also some four hole mounting operators that can be used for rear mounting switches.